Skip to main content
deep ch
Associate
March 5, 2018
Question

JTAG and Flash memory resistor calculations

  • March 5, 2018
  • 2 replies
  • 1006 views
Posted on March 05, 2018 at 11:54

JTAG and Flash memory resistor calculations

In one of the schematics. there is an 22.1 ohm series resistor between Micro controller and the Flash RAM.

Now if we go for the Stress analysis of that resistors it is going to give 0.5 W, now the question is How we can choose the value of the resistor against frequency of operation.

Kindly help me on this to understand the stress analysis perspective.

Regards,

Deepak

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    March 5, 2018
    Posted on March 05, 2018 at 14:19

    >>In one of the schematics.

    Like which one of thousands are you talking about, provide a cite.

    Typically the use of 22 or 33 ohm series resistors is to reduce over/under shoot, and ringing, on short traces driven at high slew rates. I wouldn't anticipate they would need to dissipate 1/2 Watt of power.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    deep ch
    deep chAuthor
    Associate
    March 5, 2018
    Posted on March 05, 2018 at 14:25

    Yes.. But it consumes some current..

    so we want to understand the How much current it will take and will it have a Co-relations with the Operating Frequency