Skip to main content
Kenta Chang
Associate II
February 2, 2018
Question

HOW TO SET THE BXCAN R1 AND R0 ?

  • February 2, 2018
  • 6 replies
  • 1854 views
Posted on February 02, 2018 at 18:32

Hello, 

I run the CAN loopback example project by NUCLEO-F446ZE. And find a problem, may I to set the r1 and r0 ? I read the RM0390, no message about it. Could you please let me know How to set the r1 & r0 bits?

    This topic has been closed for replies.

    6 replies

    T J
    Senior III
    February 3, 2018
    Posted on February 03, 2018 at 02:38

    I don't think you can set those bits, it looks like they are reserved by the hardware here.

    Why do you need to set those ?

    Kenta Chang
    Associate II
    February 3, 2018
    Posted on February 03, 2018 at 07:54

    When I run the Extented Remote Frame and DLC is 0, I hope to set r1 & r0  to needn't  [1] bit stuff.  If I set r0 'recessive' , and DLC is 0 , there isn't  

    [1] bit stuff.

     
    T J
    Senior III
    February 3, 2018
    Posted on February 03, 2018 at 08:06

    Why do you want to play there ?,

    R0,R1, are 'Firmware bits that are used to drive the canbus.