Skip to main content
Den In
Associate II
April 20, 2018
Question

Debugging external MCUs with STM32F746-DISCO and STM32769-DISCO

  • April 20, 2018
  • 2 replies
  • 829 views
Posted on April 20, 2018 at 15:51

Are STM32F746-DISCO and STM32769-DISCO ST-Link not supposed to be used to debug external STM32s? The T_NRST (the pin that controls the NRST pin of the target MCU) is not given out in the SWD connector, it can only be indirectly reached through the on board MCU's NRST pin. Moreover, I could not have seen any headers to cancel out the other connections between ST-Link and the on Board MCU.

Can these two boards be used to debug external MCUs and leave the on board MCU unattended while doing so?

Regards

Den

#st-link #stm32f746-disco #stm32769-disco
This topic has been closed for replies.

2 replies

Andrew Neil
Super User
April 20, 2018
Posted on April 20, 2018 at 16:01

Is it really worth the faffing about:

Both of these boards are significantly more expensive than buying a genuine standalone ST-Link;

And cheap Chinese clone ST-Links are a fraction of the price of a genuine ST-Link.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
April 20, 2018
Posted on April 20, 2018 at 17:35

>>Is it really worth the faffing about

No

I wouldn't use a $50-90 board to do external debugging, the risk of damage is high, and the alternatives cost $3-4

You could also pick a cheap Nucleo and break off the debug portion.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..