Toggling GPIOs on STM32F205RGT6
- February 7, 2018
- 13 replies
- 2609 views
Hi,
We designed a new PCB for the STM32F205RGT6, but we�re having trouble toggling GPIOs using the chip.
We wrote a simple program that toggles a GPIO every 250ms, we confirmed that the code works on the
http://www.st.com/en/evaluation-tools/nucleo-f207zg.html
and thehttp://www.st.com/en/evaluation-tools/stm3220g-eval.html
, but when we port the code to our PCB it doesn�t work.We know the code is running on the microcontroller soldered on our PCB and we know the MCU is reaching the critical section where it toggles the GPIO (because we were able to step through the code using gdb), however, for some reason we�re not seeing any change in voltage on the pin.
I attached the source code, the Makefile, and the linker script we�re using to this post. You can also check out our project on GitHub:
https://github.com/MITMotorsports/stm32f2_libs/tree/gpio_ll_cleanup/examples/gpio_ll
Any help would be much appreciated.
#stm32f205