Skip to main content
gokay aygok
Associate III
April 20, 2018
Question

The mc workbench 'MCSDK 5.0.3(2)' doesn't see STM32CUBEMX (the latest version) !!

  • April 20, 2018
  • 13 replies
  • 5359 views
Posted on April 20, 2018 at 18:33

Hello dear ST community members,

I am so sorry to ask this question for a couple of times. But, I don't have any other choice.

I have installedthe motor control workbench and STM32CUBEMX. However, I can not generate the code for motor control. The error is, NO STM32CUBEMX version above 4.0 has been found. Is there any version of cubemx which is newer than 4.0 ?

When I remove the STM32CUBEMX, I am getting the same error, too. Therefore, I came to the point that the motor control workbench MCSDK 5.0.3 and 5.0.2 do not see the latest version of cube mx, which is 4.0.

The screenshot of the error can be found in attached file.

Any help, idea, suggestion and advise would be appreciated.

Thanks a lot dear ST community members....

***I have gone through the installing steps for my all computer with windows 7 and 10 (32 and 64 bits). All results are the same.***

#cubemx #motor-control #mcsdk #pmsm #foc #sdk #need #focsdk #mc

Note: this post was migrated and contained many threaded conversations, some content may be missing.
This topic has been closed for replies.

13 replies

M. Palano
ST Employee
April 23, 2018
Posted on April 23, 2018 at 16:19

Hello dear user of x-cube-mcsdk

,

after you click/select on the [Generation] button of MCWorkbench, within the same folder where you saved the project (`<project name>.stmcx`), there should be a folder with the same exact name of the saved project. Within that folder there should be a .log file `<project name>.log`.

Can you share that log file with us?

It will help us to better understand this issue.

Best Regards.

gokay aygok
Associate III
May 2, 2018
Posted on May 02, 2018 at 19:16

Hello dear

PALANO.Carmelo_Marce

I am so happy to see your reply.

There is no such a file unfortunately.

What I have can be seen in the screenshots I will just share.

0690X0000060AwyQAE.png

0690X0000060AqRQAU.png

gokay aygok
Associate III
May 2, 2018
Posted on May 02, 2018 at 19:18

I just want to say again and again that I have downloaded, installed and uninstalled each program a lot of times.

I hope I can solve this trouble as soon as possible.

Thanks for everything in advance...

??Fil
Associate
September 27, 2018

Hello. I have the same problem and my registry does not have the entry you asked for. My cubeMX version is 4.27.0. I tried everything I found on the internet. I tried installing the softwares on three different computers, two of which are windows 10 and the other one Windows 7. In all I had the same result. Workbench cannot find cubeMX. Can you send me the .reg file if possible?

MAli.2
Visitor II
October 23, 2018

Hello. I had the same problem. Then, I fixed it by changing operating system language. If your OS has Turkish language, you get that problem. OS language must be English. Problem solved.

MYu
Associate II
June 19, 2019

I had an error. I think it failed to exccute MC workbench by java runtime error.

Failed to execute C:\Program Files\STMicroectronics\STM32CUbe\STM32CUbeMX\third_parties_plugins\com.st.stm32cube.ide.common.services.mx.jar-0.0.9.jar

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards