Skip to main content
Klavs Rommedahl
Associate II
April 27, 2018
Question

Yet a misunderstanding in RM0008

  • April 27, 2018
  • 1 reply
  • 618 views
Posted on April 27, 2018 at 13:46

Hello.

  I do Again misunderstand something in the manual RM0008.

  In Chapter 9 some port/pin settings are explained and the user can choose to have an input floating, with pull up or with pull Down. But I do not find where to choose between pull up and pull Down ???

    This topic has been closed for replies.

    1 reply

    Klavs Rommedahl
    Associate II
    May 18, 2018
    Posted on May 18, 2018 at 16:45

    As a hardware engineer it is extrem difficult for me to understand why any one would set an output bit to actually control the input bit behaviour. This is way over my head, that any one could such a stupid thing. But it actually is the case here. To control if the input pin is with Pull-Down or with Pull-Up the user actually have to set according bit in GPIOx_ODR.

    It is said in chapter 9, and when one knows what to look after it is visually clear, but confusing. And for a start not clear at all...