Skip to main content
Low Yik Seong
Associate III
April 29, 2018
Question

high side and low side pwm idle state

  • April 29, 2018
  • 1 reply
  • 661 views
Posted on April 29, 2018 at 16:41

Hi, I would like to ask what is the function of pwm idle state which can be selected in drive management in sdk 5.0? It only can be turn off as I tried turn them on they would be fatal error as I compile the code.

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards