Skip to main content
Kieron Holt
Associate II
April 25, 2018
Question

ST Link Communication Error on STM32F411

  • April 25, 2018
  • 7 replies
  • 3940 views
Posted on April 25, 2018 at 15:10

I have an STM32F411 on a PCB and I tried to connect it to the ST link using STM32 ST-Link Utility app but I get the error Cannot connect to target! Please select 'Connect Under Reset' mode from Target->Settings menu. If you are trying to connect to a discovery board, please select SWD mode from 

Target->Settings menu.' But there is no  'Connect Under Reset' mode in that menu (and the SWD mode is greyed out). In firmware version, it just says USB communication error. I have tried connecting with reset on, cycling reset, pressing the full chip erase button while reset is on then turning reset off. Nothing changes except now the error is just USB communication error. 

I then tried connecting it instead to a Nucleo-F411RE board and the same thing happened.

Any help would be great

thankyou

#st-link-v2 #st-link #nucleo-f411 #stm32-f4 #st-link-connector #st-linkv2 #stm-mcu
This topic has been closed for replies.

7 replies

Kieron Holt
Associate II
April 25, 2018
Posted on April 25, 2018 at 15:32

Some extra information: When I first connect the board the settings menu works fine with the serial number ect but then it says Old ST-Link Firmware/ST link already used but the firmware update just gives me a communication error notification. 'Communication error with ST-link. Try to start it'

Tesla DeLorean
Guru
April 25, 2018
Posted on April 25, 2018 at 17:38

Suggests something else is using it, or not in an appropriate mode to update. Unplug and replug, and do update without 'Connecting' in the ST-LINK via the Utilities. ie go straight to Firmware Update, plug in board, or reset board until it sees it. Might be a lag as different driver is required in update mode.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Kieron Holt
Associate II
April 25, 2018
Posted on April 25, 2018 at 17:44

Something else? Is using the state link or the MCU? Nothing is using either and yes I can update the firmware to the latest wersver if I go straight to the firmware updater but that hasn't made a difference. The board has been reset many times it changes nothing.

Kieron Holt
Associate II
April 25, 2018
Posted on April 25, 2018 at 15:39

It is at on firmware V2.J29.S7 (most up to date) also

Utility version: 4.2.0.0

ST link driver.dll: 5.0.3.0

ST-LINK_CLI.exe: 3.2.0.0