Skip to main content
Amir Ben Ari
Associate II
April 29, 2018
Solved

ST25 SDK fatal error on Mac OS X

  • April 29, 2018
  • 7 replies
  • 1431 views
Posted on April 29, 2018 at 16:25

Hi,

As though there are libraries available for Mac OS X, my simple application randomly (almost always) crashes, and it has something to do with the dynamic libraries provided, specifically streader.dylib.

Any thoughts would be appreciated.

I'm running a MacBook Pro with macOS High Sierra version 10.13.4.

My code:

public

static

void

main(String[]

args

)

throws

STException {

stReader

=

new

STReader();

boolean

connected

=

stReader

.connect();

connected

=

stReader

.connect();

RFGenericReader

mActiveRFReader

=

stReader

;

       

if

(

connected

) {

       

System.

out

.println(

'Connected!'

);

        

       

String

name

=

mActiveRFReader

.getName();

       

System.

out

.println(

name

+

' is connected'

);

        

       

stReader

.initialize();

       

List<

byte

[]>

uidList

=

new

ArrayList<>();

       

try

{

uidList

=

mActiveRFReader

.getTransceiveInterface().inventory(RFReaderInterface.InventoryMode.

NFC_TYPE_5

);

           

if

(!

uidList

.isEmpty()) {

               

Iso15693Command

cmd

=

new

Iso15693Command(

mActiveRFReader

.getTransceiveInterface(),

null

);

               

cmd

.setFlag(Iso15693Protocol.

HIGH_DATA_RATE_MODE

);

               

cmd

.resetToReady();

               

               

System.

out

.println(Helper.convertByteArrayToHexString(Helper.reverseByteArray(

uidList

.get(0))));

           

}

}

catch

(STException

e

) {

e

.printStackTrace();

}

        

       

}

}

Sometimes it crashes at mActiveRFReader

.getName()

[Console output]:

Connected!

#

# A fatal error has been detected by the Java Runtime Environment:

#

#

 

SIGSEGV (0xb) at pc=0x000000011081bd48, pid=6725, tid=0x0000000000002803

#

# JRE version: Java(TM) SE Runtime Environment (8.0_121-b13) (build 1.8.0_121-b13)

# Java VM: Java HotSpot(TM) 64-Bit Server VM (25.121-b13 mixed mode bsd-amd64 compressed oops)

# Problematic frame:

# C

 

[streader.dylib+0xd48]

 

Java_com_st_st25pc_model_readers_st_STReader_getName+0x18

And sometimes it crashes at  

mActiveRFReader

.getTransceiveInterface().inventory(RFReaderInterface.InventoryMode.

NFC_TYPE_5

)

[Console output]

:

Connected!

CR95HF is connected

Switching to: READER_MODE_ISO15693_MODE

#

# A fatal error has been detected by the Java Runtime Environment:

#

#

 

SIGSEGV (0xb) at pc=0x0000000120fc6dc6, pid=6714, tid=0x0000000000001803

#

# JRE version: Java(TM) SE Runtime Environment (8.0_121-b13) (build 1.8.0_121-b13)

# Java VM: Java HotSpot(TM) 64-Bit Server VM (25.121-b13 mixed mode bsd-amd64 compressed oops)

# Problematic frame:

# C

 

[streader.dylib+0xdc6]

 

Java_com_st_st25pc_model_readers_st_STReader_selectReaderMode+0x46

And sometimes I get the following, which I'm not sure what it means

[Console output]

:

Connected!

CR95HF is connected

Switching to: READER_MODE_ISO15693_MODE

=> txString 010D

<= rxString

=> txString 02A8

<= rxString

=> txString 260100

<= rxString

=> txString 060100

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

=> txString 0104

<= rxString

    This topic has been closed for replies.
    Best answer by victor laraison

    Hi amir,

    I really encourage you to switch on real CR95HF board. ST25R3911 not supported in Linux (and so MacOS) OS yet.

    BR,

    Victor

    7 replies

    victor laraison
    ST Employee
    April 30, 2018
    Posted on April 30, 2018 at 09:30

    Hi Amir,

    Please, could you provide us following information in order to reproduce issue :

    - version of ST25 NFC java application ? run Java application, then go into Help=>About. 

    We're investigating this issue, then will come back to you soon.

    thx and br,

    Vincent

    Amir Ben Ari
    Associate II
    April 30, 2018
    Posted on April 30, 2018 at 09:37

    Sorry, forgot to mention that I'm using SDK version 1.1.0.

    There's no Help => About when running the ST25 example Java app, but its the same one that comes with the 1.1.0 SDK version

    Amir Ben Ari
    Associate II
    April 30, 2018
    Posted on April 30, 2018 at 09:39

    I've run the examples Java app.

    Status of ''No reader is connected'' does not change even though Reader is attached.

    0690X0000060ApOQAU.png
    victor laraison
    ST Employee
    April 30, 2018
    Posted on April 30, 2018 at 09:55

    OK thx. I'm investigating with these information.

    stay tuned..

    Br,

    vincent

    victor laraison
    ST Employee
    May 2, 2018
    Posted on May 02, 2018 at 16:25

    hi Amir,

    I have made some tests under Eclipse/MacOS env, and it works fine at my end , with SDK1.1.0 + CR95HF.

    When you run your demo app, do you use eclipse or directly java -jar command ? 

    I will continue investigations...

    br,

    Vincent

    Amir Ben Ari
    Associate II
    May 2, 2018
    Posted on May 02, 2018 at 16:49

    Hi Victor,

    It happens both ways (Eclipse and java -jar).

    I would say that the board is NOT CR95HF, it is ST25R3911B-DISCO which for some reason is identified as CR95HF.

    Also, at another

    https://community.st.com/0D50X00009XkWOlSAN

    it was suggested that ST25R3911B is not supported on Linux any how.

    victor laraison
    ST Employee
    May 2, 2018
    Posted on May 02, 2018 at 17:10

    OK thx Amir.

    Best thing would be to send me your whole environment if possible. 

    Normally, st25R3911 is not supported yet in Linux and MacOS as libraries don't exist for Linux. I don't understand how it could be identified as CR95HF. 

    If you have got an CR95HF, it would be nice to make some tests again, then to le me know status.

    Thx and br,

    Vincent

    victor laraison
    victor laraisonBest answer
    ST Employee
    September 12, 2018

    Hi amir,

    I really encourage you to switch on real CR95HF board. ST25R3911 not supported in Linux (and so MacOS) OS yet.

    BR,

    Victor