Skip to main content
JulianH
Associate
April 27, 2018
Question

STM32F407VG + 4 bit SDIO + DMA does not work probably

  • April 27, 2018
  • 1 reply
  • 1177 views
Posted on April 27, 2018 at 19:33

Hi,

I am using the STM32F407VG and try to read an SD Card over SDIO in 4 bit mode.

I have downloaded the fatfs driver from this site:

https://community.st.com/external-link.jspa?url=http%3A%2F%2Fstm32f4-discovery.net%2F2015%2F08%2Fhal-library-20-fatfs-for-stm32fxxx%2F

The initialization works absolutely fine until the second invocation of check_fs in line 3008 of ff.c 'fmt = bsect ? check_fs(fs, bsect) : 3; /* Check the partition */'

(Note: The first invocation of check_fs in line 2998 'fmt = check_fs(fs, bsect);' returns the correct value (2))

Where it sticks after the check_fs invocation is in the interrupt of the DMA RX interrupt callback:

static void SD_DMA_RxCplt(DMA_HandleTypeDef *hdma)
{
 SD_HandleTypeDef *hsd = (SD_HandleTypeDef*)((DMA_HandleTypeDef*)hdma)->Parent;
 /* DMA transfer is complete */
 hsd->DmaTransferCplt = 1U;
 /* Wait until SD transfer is complete */
 while(hsd->SdTransferCplt == 0U)
 {
 }
 /* Disable the DMA channel */
 HAL_DMA_Abort(hdma);
 /* Transfer complete user callback */
 HAL_SD_DMA_RxCpltCallback(hsd->hdmarx); 
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

line 9 ('while(hsd->SdTransferCplt == 0U)).

Any ideas what is going wrong?

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    April 27, 2018
    Posted on April 27, 2018 at 23:36

    The DISKIO or SDIO layer isn't working properly or returning inconsistent data.

    Review current HAL examples. 

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    JulianH
    JulianHAuthor
    Associate
    May 9, 2018
    Posted on May 09, 2018 at 12:16

    Now I figured out, the second check_fs-call isn't working because theHAL_SD_IRQHandler-interrupt-function isn't setting the hsd->SdTransferCplt = 1U; due to a CRC error. So the SD_DMA_RxCplt-interrupt-functionends up in the infinite while loopwhile(hsd->SdTransferCplt == 0U).

    So my questions changed to: Why I am getting a CRC-error in the second invocation of the check_fs-function (always in the second)?

    The CRC-error check happens here:

    void HAL_SD_IRQHandler(SD_HandleTypeDef *hsd)
    { 
     /* Check for SDIO interrupt flags */
     if (__HAL_SD_SDIO_GET_FLAG(hsd, SDIO_IT_DATAEND))
     {
     __HAL_SD_SDIO_CLEAR_FLAG(hsd, SDIO_IT_DATAEND); 
     
     /* SD transfer is complete */
     hsd->SdTransferCplt = 1U;
     /* No transfer error */ 
     hsd->SdTransferErr = SD_OK;
     HAL_SD_XferCpltCallback(hsd); 
     } 
     --------> else if (__HAL_SD_SDIO_GET_FLAG(hsd, SDIO_IT_DCRCFAIL))
     {
     __HAL_SD_SDIO_CLEAR_FLAG(hsd, SDIO_FLAG_DCRCFAIL);
     
     hsd->SdTransferErr = SD_DATA_CRC_FAIL;
     
     HAL_SD_XferErrorCallback(hsd);
     
     }
     else if (__HAL_SD_SDIO_GET_FLAG(hsd, SDIO_IT_DTIMEOUT))
     {�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

    So the execution never reaches

    hsd->SdTransferCplt = 1U; and is ending up in the endless while loop.