Skip to main content
Berni Bernd
Associate
May 4, 2018
Question

STM32L072CZ Lora Keil License

  • May 4, 2018
  • 1 reply
  • 1032 views
Posted on May 04, 2018 at 13:54

Hi,

if I build the programm 'AT-Slave' (STMCubeExpansion_LRWAN) I got an License Error from Keil ( error: L6050U: The code size of this image (38072 bytes) exceeds the maximum allowed for this version of the linker.). It is possible to reduce the code size from the example without losing the function?

#at_slave #keil-mdk5 #b-l072z-lrwan1
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
May 4, 2018
Posted on May 04, 2018 at 14:35

Use the free licence

http://www2.keil.com/stmicroelectronics-stm32/mdk

 
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..