Skip to main content
Tobias Witte
Associate II
May 18, 2018
Question

ymodem problem

  • May 18, 2018
  • 0 replies
  • 897 views
Posted on May 18, 2018 at 14:18

Hello all,

I used the IAP Projekt from STM32Cube_FW_L0_V1.10.0 folder to run it on my STM32L073 NUCLEO board. Everything works fine. Now I want to implement this in my main projekt with an own pcp and an STM073VBT6. I put the needed files (common, menu, flash_if, ymodem, stm32l0xxhal_crc.c and stm32l0xxhal_crc_ex.c) in my projekt without errors. When I start the IAP-Menu and send a '1' for uploading programm, the transmission is always aborted. The terminal program (extra putty) connect with the controller, but abortet before the first package. I watched at the ''aPacketData'' Array wich get filled in the Ymodem_Receive-Function when I try to send the file project.bin:

0690X0000060KqxQAE.png

This is directly when he jumps in case 2 /* Abort by sender */. So they talk a little bit and then something goes wrong. Here is a screenshot when I upload the same file to my nucleo Board.

0690X0000060KfgQAE.png

So the first character is the only difference. Maybe someone has an idea whats going wrong? Is there a parameter in the Nocleo-Project wich I maybe forget?

Regards

Tobias

    This topic has been closed for replies.