Skip to main content
Mike Bounds
Associate
February 16, 2018
Solved

What does sim() function do

  • February 16, 2018
  • 1 reply
  • 2366 views
Posted on February 16, 2018 at 11:38

I am trying to understand what 'sim()' does in the example code that comes on the STM8L-DISCOVERY eval board (Introduction to STM8L15x power saving modes using the STM8L-DISCOVERY IDD measurement feature) where the source can be downloaded from 

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm8-embedded-software/stsw-stm8009.html

In the Project/Discover/src/icc_measure.c file in function ADC_Icc_Test it runs 'sim()' and I cannot find a definition anywhere what this function does - example:

/* Low power mode */

case MCU_LPR:

Halt_Init();

sim();

/* To prepare to start counter */

GPIO_HIGH(CTN_GPIO_PORT,CTN_CNTEN_GPIO_PIN);

/* To configure Low Power */

LPR_init();

break;

I guess this must be some built-in C function as I can't find it in any of the source or Library files, but I can't find definition on Google

Thanks

Mike

#stm8l-discovery #sim #stm8 #stm8l
    This topic has been closed for replies.
    Best answer by henry.dick
    Posted on February 16, 2018 at 12:27

    It's the c version of assembly sim instruction, opposite of rim. To disable and enable interrupts. The device header files or intrinsically should have it.

    1 reply

    henry.dick
    henry.dickBest answer
    Associate II
    February 16, 2018
    Posted on February 16, 2018 at 12:27

    It's the c version of assembly sim instruction, opposite of rim. To disable and enable interrupts. The device header files or intrinsically should have it.

    Mike Bounds
    Associate
    February 16, 2018
    Posted on February 16, 2018 at 12:49

     ,

     ,

    Thanks - I had looked in .c files in 'user' and libraries and .h files in 'user', but forgot .h files in libraries - so with your help, I have now located in ,Libraries/STM8L15x_StdPeriph_Driver/inc/stm8l15x.h :

    ♯ define rim() _rim_() /*!<,enable interrupts */

     ,

    ♯ define sim() _sim_() /*!<,disable interrupts */

    Thanks again

    Mike