Skip to main content
pj chow
Visitor II
May 17, 2018
Question

LIS3DH ADC Interrupt

  • May 17, 2018
  • 1 reply
  • 627 views
Posted on May 17, 2018 at 12:06

Hello,

    

I 

checked the lis3dh manual, there is such a sentence “

The status of the 321DA bit can be driven to the INT1 pad by setting the I1_DRY2 bit of CTRL_REG3 to 1.

� ,I have do it(ADC_PD bit of TEMP_CFG_REG (1Fh) to 1,

ODR bit of CTRL_REG1(20h)  to 1HZ ), but can’t get interruptes signals.INT1 pin is always high. other work well.

Thanks for your help.

This topic has been closed for replies.

1 reply

ST Employee
May 22, 2018
Posted on May 22, 2018 at 21:08

Can you share you complete sensor configuration so I can check it?