Skip to main content
Tomas Bengtsson
Visitor II
May 15, 2018
Question

Undershoot tolerance at STM32F767IIT6

  • May 15, 2018
  • 3 replies
  • 781 views
Posted on May 15, 2018 at 15:10

  1. Does STM32F767IIT6 tolerate an undershoot of -0.8V lasting for 2ns at a 5V tolerant I/O?
    This topic has been closed for replies.

    3 replies

    T J
    Senior III
    May 15, 2018
    Posted on May 15, 2018 at 15:55

    maybe, only because the 2nS is not enough time to overheat anything.

    You could divert that energy by using a schottky diode from ground on that pin, clamping to -0.4v max

    AvaTar
    Senior III
    May 15, 2018
    Posted on May 15, 2018 at 16:07

    maybe, only because the 2nS is not enough time to overheat anything.

    This depends on the actual circuitry 'behind the pin', I would be cautious.

    MOSFETs, for example, have a dV/dt limit. Exceeding that limit will kill it, without much energy involved (relative to it's total admissible power dissipation). I've seen FETs dying that way.

    ST Technical Moderator
    May 15, 2018
    Posted on May 15, 2018 at 15:57

    Hello

    tomas.bengtsson@prevas.se

    ,

    For the Input voltage on FT pins:VSS − 0.3V ; with maximum:VDD+4.0V

    For more details, please check therelated

    http://www.st.com/content/ccc/resource/technical/document/datasheet/group3/c5/37/9c/1d/a6/09/4e/1a/DM00273119/files/DM00273pdf/jcr:content/translations/en.DM00273pdf

    ,in the Table Voltage characteristics

    Noted that V

    IN

    maximum value must always be respected. You should refer to Table 16 for the values of the maximum allowed injected current.

    Best Regards,

    Imen.

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks