Skip to main content
antonio rueda
Associate II
February 8, 2018
Question

CAN Communication with MAT-TARGET

  • February 8, 2018
  • 1 reply
  • 704 views
Posted on February 08, 2018 at 20:41

I am trying to run a basic example using CAN with the STM32F767ZI evaluation board using the next blocks in Simulink:

0690X00000609bGQAQ.png

But when I compile the code I get the next errors:

0690X00000609YbQAI.png

Where should be all defined? I can't find any information about this or any examples. Should I change the configuration from CubeMX? Should I use another blocks to receive data?

Thanks in advance!

#can-communitation #stm32f7
This topic has been closed for replies.

1 reply

antonio rueda
Associate II
February 12, 2018
Posted on February 12, 2018 at 21:05

Fixed, it seems that the last version of the HAL drivers is not compatible with MAT-TARGET. 

CAN communication is working (after a couple of corrections on the generated code) with the last version of MAT-TARGET + STM32Cube_FW_F7_V1.8.0.