Skip to main content
Jules Patru
Associate
February 15, 2018
Question

OTP and option bytes flash banks

  • February 15, 2018
  • 1 reply
  • 684 views
Posted on February 15, 2018 at 08:33

Hello

I am developing some project using STM32L4xx microcontroller.

In technical reference manual, the chapter describing how the Flash memory behaves explains that these micro have two Flash banks. It also says that RWW operations are allowed. Thus I can use our own bootloader that sits in Bank1 to erase/write data in Flash Bank2.

In TRM §3.3.1, I can also read that Option bytes are splitted between Bank1 and Bank2 and that OTP memory is in Bank1.

Does this mean that my bootloader that sits in Bank1 can NOT write something in OTP memory?

Could you please clarify this please?

Thanks !

    This topic has been closed for replies.

    1 reply

    Doug Kehn
    Associate II
    February 15, 2018
    Posted on February 15, 2018 at 15:26

    If my understanding is correct, OTP memory can be written by code executing from Bank1. However, the MCU will stall while the OTP operation is in progress.