Skip to main content
Vijetha hn
Associate II
February 13, 2018
Solved

Pin Multiplexing details of STM32H753xI

  • February 13, 2018
  • 7 replies
  • 1888 views
Posted on February 13, 2018 at 16:26

Hi,

We are planning to use STM32H753xI in our design. We should prepare Architectural Block diagram of the Board. To do that we need to know the Pin multiplexing details of the device and accordingly plan the Interfaces in the architecture. Can you please provide the Pin multiplexing details in the form of Excel sheet or any software through which we can easily select one of  the Options out of the available Multiplexing.

Regads,

Vijetha

    This topic has been closed for replies.
    Best answer by Amel NASRI
    Posted on February 13, 2018 at 16:48

    Hi

    hn.vijetha

    ‌,

    Pins multiplexing is available in the datasheet of the product you selected,

    http://www.st.com/resource/en/datasheet/stm32h753xi.pdf

    related one in your case.

    Otherwise, you should be able to have this multiplexing in a .csv file that you get using STM32CubeMX:

    1. Open a new project to use STM32H753XI device you select from the STM32CubeMX interface
    2. Go to ''Pinout'' tab, and then select ''Generate CSV pinout text file'' as following:

    0690X00000609iuQAA.png

    -Amel

    7 replies

    Tesla DeLorean
    Guru
    February 13, 2018
    Posted on February 13, 2018 at 16:41

    I believe CubeMX provides some control and documentation output.

    If not you'll need to type the stuff in the old fashion way, or get a minion to do it. This also has the added benefit of crossing a number of neurons/synapses and providing you some knowledge instead of the robot. 

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Amel NASRI
    Amel NASRIBest answer
    ST Technical Moderator
    February 13, 2018
    Posted on February 13, 2018 at 16:48

    Hi

    hn.vijetha

    ‌,

    Pins multiplexing is available in the datasheet of the product you selected,

    http://www.st.com/resource/en/datasheet/stm32h753xi.pdf

    related one in your case.

    Otherwise, you should be able to have this multiplexing in a .csv file that you get using STM32CubeMX:

    1. Open a new project to use STM32H753XI device you select from the STM32CubeMX interface
    2. Go to ''Pinout'' tab, and then select ''Generate CSV pinout text file'' as following:

    0690X00000609iuQAA.png

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    Vijetha hn
    Associate II
    February 14, 2018
    Posted on February 14, 2018 at 13:06

    Hi,

    Is this STM32CubeMX software available as Evaluation version or we need to buy license? I want it just to check Pin Multiplexing and select the interfaces accordingly.

    Regards,

    Vijetha