Skip to main content
Brian Dahl
Associate II
February 25, 2018
Question

DMA Ringbuffer UART circular mode

  • February 25, 2018
  • 3 replies
  • 920 views
Posted on February 25, 2018 at 21:27

Hi,

i have a ringbuffer, for example an 2d Array of fixed uint8_t Bytes. It's possible that the chip at self or triggered in the Callback can update the DMA buffer address????

For example:

#define lines 8
#define bufferlinesize 36
uint8_t rxBuffer[lines][bufferlinesize]
unsigned nItrWrite=0;
.
.
.
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
nItrWrite= (nItrWrite+ 1) % lines;
huart->pRxBuffPtr = rxBuffer[nItrWriteRing];
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

#uart-dma #stm32-l4
This topic has been closed for replies.

3 replies

Tilen MAJERLE
ST Employee
February 26, 2018
Posted on February 26, 2018 at 21:20

Hello

bd

‌,

once you have RxColtCallback event, you have to start DMA read again.

HAL drivers currently don't support circular receive data over DMA.

Best regards,

Tilen

Vitaliy Chernobay
Senior
February 27, 2018
Posted on February 27, 2018 at 08:45

Hi,

Tilen MAJERLE

Why 

HAL drivers currently don't support circular receive data over DMA?

0690X00000609pWQAQ.png
Andrew Neil
Super User
February 27, 2018
Posted on February 27, 2018 at 10:32

i have a ringbuffer, for example an 2d Array

Why would a Ring buffer be a 2D array ??

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.