Associate III
April 3, 2018
Solved
STEMWIN porting on orient LCD
- April 3, 2018
- 6 replies
- 1508 views
Posted on April 03, 2018 at 07:35
Hi
i have a custom board based on stm32f769. i have interfaced orient 7inch lCD 800*480 in RGB mode. i could successfully configure the LTDC and external SDRAM (FMC based 32MB) and tried out displaying static image using layer 0. now i would like to port STEMWIN lib for my LCD and try out examples based on that. LCD has HI8264+HI8664 driver. based on the STEMWIN starting guide i configured the GUIConf.c and LCDConf.c and used GUIDRV_LIN_24 with GUICC_M888 but no luck.
i have added necessary lib for Keil as well as the STEMWIN lib components.
can anybody please suggest whether LIN driver is compatible for HI8264 / HI8664?
#lcd-interfacing