Skip to main content
Joseph Chan
Associate II
February 28, 2018
Solved

Measure current consumption by the ST25R3911B on the X-NUCLEO-NFC05A1

Posted on February 28, 2018 at 22:28

I would like to measure the current consumption during the 'Wake-up' mode with capacitive or inductive sense, and also during  the active rf-reads. Currently, the chip is powered by 5V and 3.3V. I am thinking to remove the 5V source and connect the Vdd to 3.3V as well. I can monitor the current coming from the 3.3V source. I should also remove the power LED to eliminate the current draw.

Anything else I am missing?

    This topic has been closed for replies.
    Travis Palmer
    Travis PalmerBest answer
    ST Employee
    March 6, 2018
    Posted on March 06, 2018 at 08:54

    Hi Joseph,

    This sounds like a good plan. 

    Please be aware that pin 2 and 4 of CN6 are both connected to 3.3V plane and that the power consumption in inductive wake-up and HF-field-on (

    active rf-reads)

    will be different/lower if the chip is supplied via 3.3V instead of 5V.

    BR Travis

    3 replies

    Travis Palmer
    Travis PalmerBest answer
    ST Employee
    March 6, 2018
    Posted on March 06, 2018 at 08:54

    Hi Joseph,

    This sounds like a good plan. 

    Please be aware that pin 2 and 4 of CN6 are both connected to 3.3V plane and that the power consumption in inductive wake-up and HF-field-on (

    active rf-reads)

    will be different/lower if the chip is supplied via 3.3V instead of 5V.

    BR Travis

    Joseph Chan
    Associate II
    March 19, 2018
    Posted on March 19, 2018 at 17:38

    Hi Travis,

    I made the changes as described and disconnect pin 2 on CN6. I then programmed the wake-up Timer Control Register (31h) with a value of 0 in order to observe the wake-up current. When I measure the current through the 3V3 line, I got 5.5µA, but the datasheet says 3.6µA. How can I get closer to that value?

    Thanks.

    P.S. I am using the demo firmware from 

    http://www.st.com/content/st_com/en/products/embedded-software/st25-nfc-rfid-software/x-cube-nfc5.html

    Travis Palmer
    ST Employee
    March 22, 2018
    Posted on March 22, 2018 at 10:18

    Dear Joseph

    Can you please confirm that the oscilator and mcu_clk is not turned on?

    And the following conditions are fullfilled?

    0690X0000060ACaQAM.png

    Which kind of amp-meter have you used?

    The values for this mode would be 1.6µA min, 3.6µA typical and 8µA max.

    BR Travis