2018-03-05 7:58 AM
Hi,
I'm evaluating the 3-shunt sensorless FOC (4.3.0) algorithm with STEVAL-IHM028V2 + STM32F072-EVAL.
To design my own board, I need to know the maximum - electrical - motor speed the STM32F0x at 48MHz can achieve ?
At which speed should I upgrade to F103 or higher ?
Thank you for your answer.
J. Ph.
#stm32f0 #motor-control #foc-sdk-4.3.0 #maximum-speed2018-03-13 3:01 AM
I was expecting a theoretical answer, however I performed tests and here are my results.
Speed with STM32F072, at 48MHz, flux weakening activated.
The motor I used has 2 pair of poles.
* PWM at 8kHz, FOC at 8kHz : max motor speed 13000rpm (433 Hz electrical)
-> the limit here is the algorithm
* PWM at 10kHz, FOC at 10kHz : max motor speed 17000rpm (566 Hz)
-> the limit here is my motor
2021-06-15 1:42 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards