Question
USB HS Host BenchMarks
Posted on March 06, 2018 at 23:40
Did any one test USB-HS Host throughput benchmarks for both Tx and Rx?
In device mode i am getting around 120 Mbps (both tx and rx). Even STM replied that they are seeing the same speeds. But the results don't make sense for a 480 Mbps Speed USB as it is achieving only 25 percent of bandwidth.
Platform: STM32H743xi Eval Board
Thanks.