Skip to main content
sheng yang
Senior
March 29, 2018
Question

sym32f767igt read phy chip lan8720 any register =0x00?

  • March 29, 2018
  • 1 reply
  • 1046 views
Posted on March 29, 2018 at 17:39

I try add eth support under uboot with my stm32f767igt board,my dts file as below:

ethernet_mii: mii@0 {

pins {

pinmux = <STM32F746_PG13_FUNC_ETH_MII_TXD0_ETH_RMII_TXD0>,

<STM32F746_PG14_FUNC_ETH_MII_TXD1_ETH_RMII_TXD1>,

<STM32F746_PB11_FUNC_ETH_MII_TX_EN_ETH_RMII_TX_EN>,

<STM32F746_PA2_FUNC_ETH_MDIO>,

<STM32F746_PC1_FUNC_ETH_MDC>,

<STM32F746_PA1_FUNC_ETH_MII_RX_CLK_ETH_RMII_REF_CLK>,

<STM32F746_PA7_FUNC_ETH_MII_RX_DV_ETH_RMII_CRS_DV>,

<STM32F746_PC4_FUNC_ETH_MII_RXD0_ETH_RMII_RXD0>,

<STM32F746_PC5_FUNC_ETH_MII_RXD1_ETH_RMII_RXD1>;

slew-rate = <2>;

};

};

&mac {

status = ''okay'';

pinctrl-0 = <&ethernet_mii>;

phy-mode = ''rmii'';

phy-handle = <&phy0>;

snps,reset-gpio = <&gpiof 9 1>; /*PF9<-->ETH_RESET*/

snps,reset-active-low;

snps,reset-delays-us = <1000 1000 1000>;

mdio0 {

#address-cells = <1>;

#size-cells = <0>;

compatible = ''snps,dwmac-mdio'';

phy0: ethernet-phy@0 {

reg = <0>;

};

};

};

i conformed mdio relate pin PC1 and PA2 with AF11 function as below

0690X0000060AIjQAM.png

and GPIOC and GPIOA are enabled as

0690X0000060AJqQAM.png

but whichever register of the phy chip i read i always get 0x0000,,,

0690X0000060AJRQA2.png

i try use mii info command test again ,i get the same 

0690X0000060AJWQA2.png

Besides,once i insert the cable to router,the link on rj45 both light,but i could not ping server success.

what's wrong maybe?

    This topic has been closed for replies.

    1 reply

    sheng yang
    Senior
    March 30, 2018
    Posted on March 30, 2018 at 17:54

    after i change a phy chip lan8720a,now i could get registers in this phy,as below

    0690X0000060AKoQAM.png

    but when i try to test the net , i get this message

    0690X0000060AKtQAM.png

    and i see hal code,in func HAL_StatusTypeDef HAL_ETH_Init(ETH_HandleTypeDef *heth)

    there is some code just like

    tickstart = HAL_GetTick();

    #if 1

    /* Wait for software reset */

    while (((heth->Instance)->DMABMR & ETH_DMABMR_SR) != (uint32_t)RESET)

    {

    /* Check for the Timeout */

    tickstart = HAL_GetTick();

    if((HAL_GetTick() - tickstart ) > ETH_TIMEOUT_SWRESET)

    {

    heth->State= HAL_ETH_STATE_TIMEOUT;

    /* Process Unlocked */

    __HAL_UNLOCK(heth);

    /* Note: The SWR is not performed if the ETH_RX_CLK or the ETH_TX_CLK are

    not available, please check your external PHY or the IO configuration */

    return HAL_TIMEOUT;

    }

    }

    #endif

    As the comment said 

    The SWR is not performed if the ETH_RX_CLK or the ETH_TX_CLK are

    not available, please check your external PHY or the IO configuration.

    what's the ETH_TX_CLK or ETH_RX_CLK,i could not get these pins in phy chip lan8720a,the pins of lan8720a just below

    0690X0000060ALDQA2.png

    is these pins of ETH_TX_CLK and ETH_RX_CLK be relate with pin5 and pin14??