Skip to main content
shammi d
Associate II
December 12, 2017
Question

sending data from STM32 LoRa discovery kit

  • December 12, 2017
  • 5 replies
  • 1069 views
Posted on December 12, 2017 at 07:18

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    December 15, 2017
    Posted on December 15, 2017 at 17:24

    This seems to be pretty remedial level stuff.

    Remove or comment out the PRINTF() statements in sx1276.c to get rid of the txDone, rxDone and rxTimeOut messages, and those in main.c generating the OnTxDone, OnRxDone , OnRxTimeout, OnTxTimeout, OnRxError, etc

    Replace with PRINTF() of your choice and construction. The data is output/buffered by code in vcom.c

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Norhane BENKAHLA
    Associate II
    January 26, 2018
    Posted on January 26, 2018 at 12:50

    hi , please in which part of script can i change the message? i can't see in which part the message is generated 

    thanks

    Tesla DeLorean
    Guru
    January 26, 2018
    Posted on January 26, 2018 at 13:56

    These messages? Use the 'Find in Files' search mode of your IDE to locate them.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Andrew Neil
    Super User
    December 15, 2017
    Posted on December 15, 2017 at 19:07

    As ​ says, these are just PRINTFs - you can simply add and remove them as you see fit.

    But note that they are only sending across the local USB link - not the LoRa radio link ...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.