Skip to main content
Jonas L
Associate
December 9, 2017
Question

STM32 and VL53L0X

  • December 9, 2017
  • 3 replies
  • 1307 views
Posted on December 09, 2017 at 19:30

Hey there,

I'm working with my STM32L476 and the VL53L0X rangngs sensor.

I'm using the Example from X-CUBE-53L0A1. I don't have the Nucleo board for the Sensor just a satellite board.  When using the example for ranging with the example 'RangingWithSatellites'  I get the error shown in the picture. What am I doing wrong.

The sensor is connected correctly, and the program should work.

Thanks for the help.

#vl53l0x #stm32l476
This topic has been closed for replies.

3 replies

Andrew Neil
Super User
December 11, 2017
Posted on December 11, 2017 at 11:38

Could you not have embedded that picture - so that we could actually see it, without having to separately open it?

Jonas L wrote:

The sensor is connected correctly, and the program should work.

But the message is complaining about an I2C Expander - not the sensor - isn't it?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Jonas L
Jonas LAuthor
Associate
December 11, 2017
Posted on December 11, 2017 at 12:16

It looks like it does. I don't really understand the error.

John E KVAM
ST Employee
January 2, 2018
Posted on January 02, 2018 at 16:55

The ST Expansion board has in addition to the sensor, an LED 4 digit display. This display uses a lot of PIOs and requires the use of a PIO Expander. Unfortuately the PIOs are not connected directly to the Sensor, but go through the Expander. Hence you are talking to a device that is not on your system.

Two choices are to buy the ST VL53 Expander board, or two dig into the code and remove the bits that talk to the PIO expander board and talk to the Sensor directly.

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.