Skip to main content
Scott Deyo
Visitor II
December 11, 2017
Question

STBC03 Eval Kit Manual (and Board?) Error

  • December 11, 2017
  • 0 replies
  • 462 views
Posted on December 11, 2017 at 19:55

In the STEVAL-ISB035V1 Manual (UM2132), the schematic and ball-out refer to the STBC02 instead of the -03.

Also, on the board, both R11 (in the '02' section') and R8/ R13 (in the '03' section) are installed. This doesn't seem right, since BATMS_EN should be high or low, not divided.

A hyperlink in datasheets would be useful for reporting mistakes.

#stbc03
This topic has been closed for replies.