Question
UART baudrate problem
Posted on April 08, 2018 at 20:15


Hello,
I try to send data via UART with a baudrate 8Mb/s using
Nucleo-L476RG and UM232H,
the programs I use are
STM32CubeMx and Putty (for RX)
As shown on the picture below we can send data
via
USART1
with a baudrate between 2.443Kbits/s and 10Mb/s
but in reality when I exceed 1Mb/s ,I don't recieve any information in RX,
Probably, it is a speed interval problem generated in code as shown on the pictures below, I think, there is a bad coordination between the configuration and the code,

This is the declaration part :

Can any one help me please!
Thanks in advance