Skip to main content
Evgeny Boltunov
Associate
July 4, 2018
Question

BluNRG-1 lower power consumption

  • July 4, 2018
  • 1 reply
  • 686 views
Posted on July 04, 2018 at 12:44

Hello,

I am using BluNRG-1 module with Stack v1.0.

My clock source is 'LS_SOURCE = LS_SOURCE_INTERNAL_RO', the module has no external oscillator.

I used the following code to lower the power consumption, as it is adviced in 'BlueNRG-1 and BlueNRG-2 low power modes.pdf' and I am getting average current consumption about 120 uA.

BlueNRG_Sleep(SLEEPMODE_WAKETIMER,

WAKEUP_IO13,

WAKEUP_IO_LOW,

0);

I also tried 

SLEEPMODE_NO

TIMER option with the same current consumption: 120 uA.

The advertising interval in my application has been set to 1000 ms.

Can you please advice, what setting will make the power consumption below 20 uA?

In advance thanks,

Evgeny

#bluenrg-1 #sleep-mode
This topic has been closed for replies.

1 reply

Michael Krechko
Associate
July 6, 2018
Posted on July 06, 2018 at 22:29

As a first step I advise to use this software 

https://www.st.com/en/embedded-software/stsw-bnrg001.html

  write your connection settings then compare it with measurement. What equipment do you use for measurement?