Skip to main content
Martin Sigrand
Associate
April 19, 2018
Question

Can't get the STM32H753 ADC to work with DMA in cubemx

  • April 19, 2018
  • 2 replies
  • 1062 views
Posted on April 19, 2018 at 15:45

I try to configure ADC + DMA continues cicrcular mode for a H753eval board with CubeMX but with no success.

The example en.stm32cubeh7\STM32Cube_FW_H7_V1.2.0\Projects\STM32H743I_EVAL\Examples\ADC\ADC_DMA_Transfer works perfect but as I have started using cubemx for my other peripherals I would like to stay with cubemx, but I don't get it to work with the ADC+DMA.

Now I have backed to a completely clean project for a 753XI, only configured ADC1_IN0 and RCC(25MHz->400MHz sysclk and 18.75MHz ADC clk).

When I run it as ADC con't mode without DMA

0690X0000060AgBQAU.png

and add the following to my main.c, everything works.

#include ''main.h''

#include ''stm32h7xx_hal.h''

ADC_HandleTypeDef hadc1;

uint16_t adcData;

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_ADC1_Init(void);

int main(void)

{

HAL_Init();

SystemClock_Config();

MX_GPIO_Init();

MX_ADC1_Init();

HAL_ADC_Start(&hadc1);

while (1)

{

adcData = HAL_ADC_GetValue(&hadc1);

But when I change ADC1 config in cubemx to:

0690X0000060AgGQAU.png

added a DMA1 stream0, with circular mode and changed the rows in my code to:

ALIGN_32BYTES (static uint16_t adcData[32] );

HAL_ADC_Start_DMA(&hadc1,(uint32_t*)adcData,32)

and no code in main()

Nothing works! If a check adc.dr register with the debugger it only takes one value at start-up and nothing more.

I've also fiddled with the Conversion Data Management mode as that parameter is a little unclear to me, circular mode is set in the DMA tab as well and the youtube clips I have seen is using older parts/version which doesn't have that setting.

I've also tried for hours to compare the code generated with the one in the Project/__ /Example to find the problem but without success.

using cubemx 4.25.0

Some ideas anyone??

Thx / Martin

    This topic has been closed for replies.

    2 replies

    Martin Sigrand
    Associate
    April 20, 2018
    Posted on April 20, 2018 at 11:45

    Solution found: cubemx, at least for H753 and EWARM generates 0x20000000 as default RAM area in the linker file(stm32h753xx_flash.icf) and that is the DTCM-RAM which is not accessible from the standard DMA. 

    Where is the ICF editor referred to below, I did edit the file for now!

    /*###ICF### Section handled by ICF editor, don't touch! ****/

    /*-Editor annotation file-*/

    /* IcfEditorFile='$TOOLKIT_DIR$\config\ide\IcfEditor\cortex_v1_0.xml' */

    /*-Specials-*/

    define symbol __ICFEDIT_intvec_start__ = 0x08000000;

    /*-Memory Regions-*/

    define symbol __ICFEDIT_region_ROM_start__ = 0x08000000;

    define symbol __ICFEDIT_region_ROM_end__ = 0x081FFFFF;

    /*define symbol __ICFEDIT_region_RAM_start__ = 0x20000000;

    define symbol __ICFEDIT_region_RAM_end__ = 0x2001FFFF;*/

    define symbol __ICFEDIT_region_RAM_start__ = 0x24000000;

    define symbol __ICFEDIT_region_RAM_end__ = 0x2407FFFF;

    define symbol __ICFEDIT_region_ITCMRAM_start__ = 0x00000000;

    define symbol __ICFEDIT_region_ITCMRAM_end__ = 0x0000FFFF;

    /*-Sizes-*/

    define symbol __ICFEDIT_size_cstack__ = 0x400;

    define symbol __ICFEDIT_size_heap__ = 0x200;

    /**** End of ICF editor section. ###ICF###*/

    define memory mem with size = 4G;

    define region ROM_region = mem:[from __ICFEDIT_region_ROM_start__ to __ICFEDIT_region_ROM_end__];

    define region RAM_region = mem:[from __ICFEDIT_region_RAM_start__ to __ICFEDIT_region_RAM_end__];

    define region ITCMRAM_region = mem:[from __ICFEDIT_region_ITCMRAM_start__ to __ICFEDIT_region_ITCMRAM_end__];

    define block CSTACK with alignment = 8, size = __ICFEDIT_size_cstack__ { };

    define block HEAP with alignment = 8, size = __ICFEDIT_size_heap__ { };

    initialize by copy { readwrite };

    do not initialize { section .noinit };

    place at address mem:__ICFEDIT_intvec_start__ { readonly section .intvec };

    place in ROM_region { readonly };

    place in RAM_region { readwrite,

    block CSTACK, block HEAP };
    Tesla DeLorean
    Guru
    April 20, 2018
    Posted on April 20, 2018 at 13:40

    >>the DTCM-RAM which is not accessible from the standard DMA. 

    Diagramming suggest the plumbing is there, and the DTCM-RAM is viable for SDMMC DMA operation, which is less problematic from a caching/sharing/coherency standpoint

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..