Skip to main content
Maurice Jackson
Visitor II
April 21, 2018
Question

stm32f446e-eval board bootloader

  • April 21, 2018
  • 1 reply
  • 669 views
Posted on April 22, 2018 at 00:19

I just received my brand new STM32446E-EVAL board and the first thing I tried to use was in the In-System bootloader.  My problem is that the ''Flash Loader Demonstrator'' utility never connects to the mcu.  I keep the getting a ''No response from the target, the Bootloader can not be started ...'' .  I double checked that Boot1 = 0, Boot0 = 1, and  all my COM settings.  I must be missing something.  Any help would be greatly appreciated.  I still need to check the flash protection level,... I new to this mcu so I need to figure out how to accomplish this.

0690X0000060AdhQAE.png

Thank you,

Kenneth

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    April 22, 2018
    Posted on April 22, 2018 at 22:53

    Is it connecting to the right USART? The System-Loader has limited connectivity, and sensitive to transitions on interfaces it is watching.

    Perhaps try the USB-FS connector and see if it comes up in DFU mode.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..