Question
cubef4 STM32F4-Discovery dac example problem?
Posted on April 27, 2018 at 15:04
hi
i want use DAC_SignalsGeneration example for Making waveforms in my stm32f407 discovery eval board
i
redefine
const uint8_t aEscalator8bit[6] = {0x0, 0x33, 0x66, 0x99, 0xCC, 0xFF};
to
const uint16_t aEscalator16bit[100]={82,164,246,328,410,492,573,655,
737,819,901,983,1065,1147,1229,1311,1393,1475,1556,1638,1720,1802,1884,1966,2048,2130,2212,2294,2376,2458,2540,2621,2703,2785,2867,2949,3031,3113,3195,3277,3359,3441,3523,3604,3686,3768,3850,3932,4014,4096,4014,3932,3850,3768,3686,3604,3523,3441,3359,3277,3195,3113,3031,2949,2867,2785,2703,2621,2540,2458,2376,2294,2212,2130,2048,1966,1884,1802,1720,1638,1556,1475,1393,1311,1229,1147,1065,983,901,819,737,655,573,492,410,328,246,164,82,0};and change DAC_ALIGN_8B_R to DAC_ALIGN_12B_R in this line
/*##-2- Enable DAC Channel1 and associated DMA #############################*/
if(HAL_DAC_Start_DMA(&DacHandle, DACx_CHANNEL1, (uint32_t*)aEscalator16bit, 100,DAC_ALIGN_12B_R
) != HAL_OK) { /* Start DMA Error */ Error_Handler(); }}but my
Generated
waveform is disordered in the oscilloscope.i need to 12bit dac.where is my problem?