Skip to main content
HAMADI Gratien
Visitor II
January 16, 2018
Question

Can you confirm that the STM32F4 is pin-to-pin compatible with the STM32L4 please ?

  • January 16, 2018
  • 1 reply
  • 976 views
Posted on January 16, 2018 at 11:00

http://www.st.com/en/microcontrollers/stm32l4-series.html?querycriteria=productId=SS1580

 

'

To simplify migration and give you all the flexibility you need, the STM32L4 is pin-to-pin compatible with the different STM32 series and opens the door to the full STM32 ecosystem.'

    This topic has been closed for replies.

    1 reply

    Bogdan Golab
    Lead
    January 16, 2018
    Posted on January 16, 2018 at 11:53

    This docs might be interesting:

    http://www.st.com/content/ccc/resource/technical/document/application_note/group0/02/46/be/cf/31/75/4e/de/DM00263732/files/DM00263732.pdf/jcr:content/translations/en.DM00263732.pdf

     

    '

    STM32L4 Series / STM32L4+ Series as well as STM32F405/415 and STM32F407/417 lines

    share a high level of

    pin

    compatibility.

    Most peripherals share the same

    pin

    s.

    The transition from STM32F405/415 and STM32F407/417 lines to STM32L4 Series /

    STM32L4+ Series is simple since only a few

    pin

    s are different.'