Associate II
Jun 24, 2018 8:47 PM UTC
Solved
Flash Download failed - Could not load file .axf Issue
- 5 replies
- 18469 views
Posted on June 24, 2018 at 22:47
Hi,
When I compile a project, I get an error: '.\Objects\uygulama1.axf' - 1 Error(s), 0 Warning(s). Target not created. Then I click Download, I get an error: 'Flash Download failed - Could not load file'
I tried to solve many times and searched on the internet, however it couldn't help me to fix the issue.
I wonder why Keil can not make xxx.axf file. I use
MDK-ARM Version 5.25
I also have a project which has an .axf file. On my project, .axf the couldn't found. So I copied the file from the project I have. I renamed the .axf file as 'uygulama1.axf'. This clearly worked.
But I would like to fix the issue for the next projects.
You can see the issue screenshots below.
Thanks in advance.
#flash-download-failed #target-not-created