Question
DAP access to SRAM
Posted on May 08, 2018 at 22:52
Hi -
Is it possible for a debugger to directly r/w to embedded SRAM via one of the debug APs (access ports) on the
♯
That is, I don't want to access SRAM via the M7 since the &sharpcache might be enabled. I'd like to inspect SRAM contents, not the cache.According to the TRM, AP0 is dedicated to the M7, so I assume SRAM access will be through the M7/cache. AP1 (D3 AHB interconnect) looks right, but I did some experiments that suggesting that access is also through M7. Could someone clarify?
Regards, Ted.
#stm32h7x3? #stm32h7x3