Skip to main content
Damiano Balzani
Associate II
February 2, 2018
Solved

IWDG (Watchdog) Enable on STM32

  • February 2, 2018
  • 6 replies
  • 2099 views
Posted on February 02, 2018 at 09:21

Hi everybody,

i'm tryng to configure the IWDG but it doesn't work. i didn't find the enable bit, is there?

Can you help me?

I post my code here

void wdt_enable(void)

{

RCC -> CSR = RCC -> CSR | 0x00000001; //Enable LSI Clock

while((RCC -> CSR & 0x02)==0)

{

//add timeout code here

}

IWDG -> KR = 0x0000CCCC; //Enable IWDG

IWDG -> KR = 0x00005555; //Enable register access

IWDG -> PR = 0x010; //Set Prescaler /16

IWDG -> RLR = 0xFFF; //Set Reload Value for 2.048 seconds

while(IWDG -> SR) //Check if flags are reset

{

//add timeout code here

}

IWDG -> KR = 0x0000AAAA; //Refresh the counter

}

Thanks in advance

Damiano

#stm32-iwdg #iwdg
This topic has been closed for replies.
Best answer by waclawek.jan
Posted on February 02, 2018 at 14:09

Which register?

IWDG_KR is write only, ie. reading it back is not defined (probably results in 0).

IWDG_PR and IWDG_RLR have this note - read the IWDG chapter in RM:

Note: Reading this register returns the reload value from the VDD voltage domain. This value

may not be up to date/valid if a write operation to this register is ongoing on this

register. For this reason the value read from this register is valid only when the RVU bit

in the IWDG_SR register is reset.

JW

6 replies

henry.dick
Associate II
February 2, 2018
Posted on February 02, 2018 at 13:49

'

i didn't find the enable bit, is there?'

have you read the code you have written? it explicitly does so.

waclawek.jan
Super User
February 2, 2018
Posted on February 02, 2018 at 13:56

it doesn't work

How do you know?

i didn't find the enable bit

There is no enable bit - writing the key value CCCCh starts the watchdog

JW

Damiano Balzani
Associate II
February 2, 2018
Posted on February 02, 2018 at 14:04

because i'm using a debugger and i'm seeing that the registers have not the value written in the code

do i miss something?

Thanks

DB

henry.dick
Associate II
February 2, 2018
Posted on February 02, 2018 at 14:09

'because i'm using a debugger and i'm seeing that the registers have not the value written in the code'

that's a different question.

'do i miss something?'

read the datasheet, as it is designed to answer this sort of questions: it has a section specifically on that.