Skip to main content
Shi gan
Visitor II
May 8, 2018
Solved

st25ru3993 the program demo

  • May 8, 2018
  • 1 reply
  • 582 views
Posted on May 08, 2018 at 08:26

st25ru3993 the program demo

void gen2Select(gen2SelectParams_t *p)

{ buf_[i] |= ((p->truncation<<3)&0x08); /* Truncate */}

how to use p->truncation,i do not known its meaning.

    This topic has been closed for replies.
    Best answer by Finnley Harris
    Posted on June 04, 2018 at 09:43

    The truncation is implemented based on Gen2 standard, from Gen2 2.0.1 protocol standard document, 6.3.2.12.1.1 (Description of mandatory Select command):

    [...]Truncate indicates whether a Tag’s backscattered reply shall be truncated to those EPC bits that follow

    Mask. If an Interrogator asserts Truncate, and if a subsequent Query specifies Sel=10 or Sel=11, then a

    matching Tag shall truncate its ACK reply to the portion of the EPC immediately following Mask, followed

    by a PacketCRC[...]

    In other words it is used to reduce the payload size of the tag reply by masking part of its EPC ID.

    In our firmware the truncation parameter for select is set via a GUI command:

    In selectTag(),

    appl_commands.c

    :

    selParams[idx].truncation = cmdBuffer.rxData[7];

    In the current GUI there is no control to set the truncation, but the functionality behind is done.

    An example setting of truncation could be done e.g. by adding the following

    line

    to the code:

    In STReader::selectTag(),

    STReader.cpp

    :

    TagSelect selCmd(TagSelect::Clear_and_add);

    selCmd.setTarget(m_Session);

    selCmd.setAction(m_Action);

    selCmd.setAddr(m_Addr);

    selCmd.setTruncation(1);

    1 reply

    Finnley Harris
    Finnley HarrisBest answer
    ST Employee
    June 4, 2018
    Posted on June 04, 2018 at 09:43

    The truncation is implemented based on Gen2 standard, from Gen2 2.0.1 protocol standard document, 6.3.2.12.1.1 (Description of mandatory Select command):

    [...]Truncate indicates whether a Tag’s backscattered reply shall be truncated to those EPC bits that follow

    Mask. If an Interrogator asserts Truncate, and if a subsequent Query specifies Sel=10 or Sel=11, then a

    matching Tag shall truncate its ACK reply to the portion of the EPC immediately following Mask, followed

    by a PacketCRC[...]

    In other words it is used to reduce the payload size of the tag reply by masking part of its EPC ID.

    In our firmware the truncation parameter for select is set via a GUI command:

    In selectTag(),

    appl_commands.c

    :

    selParams[idx].truncation = cmdBuffer.rxData[7];

    In the current GUI there is no control to set the truncation, but the functionality behind is done.

    An example setting of truncation could be done e.g. by adding the following

    line

    to the code:

    In STReader::selectTag(),

    STReader.cpp

    :

    TagSelect selCmd(TagSelect::Clear_and_add);

    selCmd.setTarget(m_Session);

    selCmd.setAction(m_Action);

    selCmd.setAddr(m_Addr);

    selCmd.setTruncation(1);