Skip to main content
Alpha Mr
Associate II
May 16, 2018
Question

SWSTM32 build errors

  • May 16, 2018
  • 5 replies
  • 1538 views
Posted on May 16, 2018 at 08:04

Hi,

I am exploring X-NUCLEO_IDB05A1 with STM32L476RG Nucleo, And while building the Profile_central project, I am getting build errors in console. Errors like:

arm-none-eabi-gcc: error: ..\..\..\..\..\..\..\..\Middlewares\ST\STM32_BlueNRG\LibProfCentr\Src\proximity_reporter\proximity_reporter.c: No such file or directory

arm-none-eabi-gcc: fatal error: no input files

compilation terminated.

Every time it displays different file names in above error. Those files are there but still it says that it didn't found the files! I know Eclipse gives error for deep addresses, so I extracted the en.X-CUBE-BLE1 to desktop but still it gives the same errors.

Anybody know how to solve this error?

#swst32
    This topic has been closed for replies.

    5 replies

    AvaTar
    Senior III
    May 16, 2018
    Posted on May 16, 2018 at 09:12

    Those files are there but still it says that it didn't found the files!

    You seeing it in the file manager doesn't mean the compiler sees it.

    I know Eclipse gives error for deep addresses, ...

    Why do you believe that ?

    ... so I extracted the en.X-CUBE-BLE1 to desktop but still it gives the same errors.

    There is no 'desktop'. This is just a graphical GUI metaphor.

    Do you know where in the file system those files really end up when you 'extract to the desktop' ?

    arm-none-eabi-gcc: error: ..\..\..\..\..\..\..\..\Middlewares\ST\STM32_BlueNRG\LibProfCentr\Src\proximity_reporter\proximity_reporter.c: No such file or directory

    Do you know what that path string means, and have you checked it with a file manager ?

    Alpha Mr
    Alpha MrAuthor
    Associate II
    May 16, 2018
    Posted on May 16, 2018 at 09:25

    You seeing it in the file manager doesn't mean the compiler sees it.

    I mean, by opening a declaration I have confirmed that IDE knows that where the files are. If it don't then it won't have shown me the file by pressing F3 key, isn't it?

    Why do you believe that ?

    Actually I have tested the SensorDemo project of this package. And it gave same errors when the project was in deep location, so I pasted that project in narrow location and it build and worked fine. Hence I believe.

    There is no 'desktop'. This is just a graphical GUI metaphor.

    Do you know where in the file system those files really end up when you 'extract to the desktop' ?

    Yes. But I thought desktop would be less deep location to avoid errors. Yes I know where the files are and yes they really end up where I extracted them.

    Do you know what that path string means, and have you checked it with a file manager ?

    Yes I have tested this path and the file is actually there.

    Thanks.

    AvaTar
    Senior III
    May 16, 2018
    Posted on May 16, 2018 at 10:34

    I mean, by opening a declaration I have confirmed that IDE knows that where the files are. If it don't then it won't have shown me the file by pressing F3 key, isn't it?

    You mix up the IDE with the compiler. Open files in the editor does not add them to the project.

    Yes. But I thought desktop would be less deep location to avoid errors. Yes I know where the files are and yes they really end up where I extracted them.

    ...

    Yes I have tested this path and the file is actually there.

    I suppose you work on a Windows system.

    Do you have spaces or special characters in path names ?

    File systems on Mac and Linux systems are case-sensitive.

    Get your toolchain to display a full build console log (inlcuding the build command line), and check what paths this actually evaluates to.