Skip to main content
Jacek Pieczaba
Associate III
July 10, 2018
Question

Vibration measurements

  • July 10, 2018
  • 2 replies
  • 651 views
Posted on July 10, 2018 at 13:52

Hello,

I would like to ask you for suggestion. I would like to monitor vibration of the motor in my system. What should I use MEMS microphone or 3-axis  Accelerometer  or Both? I am using stepper motor to  drive a pump and I would like to monitor the behavior of entire assembly. I have found an latest reference design STEVAL-IDP005V1 which contain both 

 IIS2DH ( 3-axis Accelerometer ) and MP34DT05 ( mems microphone ). Could you explain me why on the reference design are both sensors and is there any specific software which based on the sensor input notify system about specific behavior? 

Thanks a lot in advnace

Jacek 

This topic has been closed for replies.

2 replies

ST Employee
July 13, 2018
Posted on July 13, 2018 at 11:29

It depends which kind of issues you want to detect, each different issue produce different frequencies.

Accelerometer is used up to ones of kHz and microphone up to tens of kHz.

See following chart.

0690X0000060MBhQAM.png
Jacek Pieczaba
Associate III
July 13, 2018
Posted on July 13, 2018 at 22:40

Thanks a lot Miroslav for answer really appreciate now I understand why both sensors was placed on the board ( to cover as much as possible failure ranges ). I think so I will try first to stay with ISM330DLC and see how much issues I can catch using it. 

Thank you again

Jacek