Skip to main content
Pablito Parseval
Associate II
February 15, 2018
Question

PWM FORCED ACTIVE

  • February 15, 2018
  • 5 replies
  • 1603 views
Posted on February 15, 2018 at 09:32

Hi All,

in my application, i need sometimes to stop PWM and Force Output to High.

I write this code but seem not run good. 

void forcePwmActive(void)

{

   TIM_OC_InitTypeDef configOC;

   HAL_TIM_PWM_Stop(&htim21, TIM_CHANNEL_2);

   configOC.OCMode = TIM_OCMODE_FORCED_ACTIVE;

   configOC.Pulse = 0;

   configOC.OCPolarity = TIM_OCPOLARITY_HIGH;

   configOC.OCFastMode = TIM_OCFAST_DISABLE;

   if(HAL_TIM_OC_ConfigChannel(&htim21, &configOC, TIM_CHANNEL_2) != HAL_OK)

   {

      _Error_Handler(__FILE__, __LINE__);

   }

}

Can anyone help?

    This topic has been closed for replies.

    5 replies

    waclawek.jan
    Super User
    February 15, 2018
    Posted on February 15, 2018 at 09:51

    What are the symptoms?

    What's the content of TIM21 registers?

    JW

    Pablito Parseval
    Associate II
    February 15, 2018
    Posted on February 15, 2018 at 11:18

    The TIM Setup is the following:

    void systemConfig_TIM21Setup(void)

    {

       TIM_ClockConfigTypeDef sClockSourceConfig;

       TIM_MasterConfigTypeDef sMasterConfig;

       TIM_OC_InitTypeDef sConfigOC;

       htim21.Instance = TIM21;

       htim21.Init.Prescaler = 0;

       htim21.Init.CounterMode = TIM_COUNTERMODE_CENTERALIGNED3;

       htim21.Init.Period = 16000;

       htim21.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

       if (HAL_TIM_Base_Init(&htim21) != HAL_OK)

       {

       _Error_Handler(__FILE__, __LINE__);

       }

       sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;

       if (HAL_TIM_ConfigClockSource(&htim21, &sClockSourceConfig) != HAL_OK)

       {

          _Error_Handler(__FILE__, __LINE__);

       }

       if (HAL_TIM_PWM_Init(&htim21) != HAL_OK)

       {

          _Error_Handler(__FILE__, __LINE__);

       }   

       sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

       sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

       if (HAL_TIMEx_MasterConfigSynchronization(&htim21, &sMasterConfig) != HAL_OK)

       {

          _Error_Handler(__FILE__, __LINE__);

       }

          sConfigOC.OCMode = TIM_OCMODE_PWM1;

          sConfigOC.Pulse = 0;

          sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;

          sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;

       if (HAL_TIM_PWM_ConfigChannel(&htim21, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)

       {

          _Error_Handler(__FILE__, __LINE__);

       }

       HAL_TIM_MspPostInit(&htim21);

    }

    The effect is that if i measure with the oscilloscope the PWM output, is not forced to HIGH.

    waclawek.jan
    Super User
    February 15, 2018
    Posted on February 15, 2018 at 13:08

    What's the content of TIM21 registers (after the 'forcing' routine)?

    Read them out in debugger and post.

    JW

    Pablito Parseval
    Associate II
    February 15, 2018
    Posted on February 15, 2018 at 13:19

    Like you can see in the image below, the CCMR1 register have the bit [14:12] set to 101 like required 

    in the datasheet.

    0690X00000609loQAA.png
    waclawek.jan
    Super User
    February 15, 2018
    Posted on February 15, 2018 at 14:30

    Yes indeed, but also CCER is all zero which means the CCxE bits are cleared.

    Try to set them.

    JW