The elf loader file is not accessible [only via *.bat]
Hello everybody,
i have a strange problem, hope that someone has a great idea what i can do...
We have custom board's with the stm32f7 and f4. Normaly we flash the device via bat (or open ocd(which is working)).
The bat looks like this:
..\st-link\ST-LINK_CLI.exe -c SWD UR -Rst
..\st-link\ST-LINK_CLI.exe -c SWD UR -P firmware.hex..\st-link\ST-LINK_CLI.exe -c SWD UR -P bootloader.hex..\st-link\ST-LINK_CLI.exe -c SWD UR -Rstpause
Since someday's i get the follow error message while flashing:
The elf loader file is not accessible.
This is the complete output from the console:
ST-LINK SN : 33FF68064D4E353545150843
ST-LINK Firmware version : V2J24S4Connected via SWD.SWD Frequency = 4000K.Target voltage = 3.2 V.Connection mode : Connect Under Reset.Device ID:0x449Device flash Size : 512 KbytesDevice family :STM32F74x/F75xLoading file...
Flash Programming: File : firmware.hex Address : 0x00200000Memory programming...?????????????????????????????????????????????????? 0%The elf loader file is not accessible.We have this problem on two PC's and one PC is working.
I already tried:
Flashing via St-Utility -> Working without a problem
Flashing via openocd ->
Working without a problem
SWD Frequenz to 1800K -> Same problem
Updated St-Utility
-> Same problem
Firmware Update the St-Link
-> Same problem
Take a Brandnew ST-Link
-> Same problem
Updated Win driver
-> Same problem
Taking the st-link from the pc which is working
-> Same problem
What can i do or try?
If you know something i would be very happy
Thank you and have a nice day!
#loader #elf #bat