Skip to main content
Dennis Chou
Associate
February 16, 2018
Question

where is the STM32F107xx IEEE 1588 PTPd package?

  • February 16, 2018
  • 22 replies
  • 6354 views
Posted on February 16, 2018 at 18:55

Where can I download the 

STM32F107xx lwIP stack with IEEE 1588 PTPd support? I have read the application notes AN3102 and AN3411, and the 3411 note appear to indicate there is a PTPd port for this line of processors.

Thanks

Dennis

#stm32f107xx-ptp-ieee-1588
This topic has been closed for replies.

22 replies

Szymon PANECKI
Senior III
February 17, 2018
Posted on February 17, 2018 at 09:42

Hello Dennis,

I can't find AN3411 on ST website. Could you please check again the name of application note?

Regarding AN3102, software related to this application note is available here:

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-standard-peripheral-library-expansion/stsw-stm32026.html

.

Regards

Szymon

Kamil Alkhouri
Associate II
April 17, 2018
Posted on April 17, 2018 at 12:51

Dear Szymon,

I have the same problem so I thought it would be helpful to discuss it with you.

For some reason, the application note AN3411 is not available on ST website anymore, however you can find it on:

http://www.bdtic.com/download/ST/AN3411.pdf

 

How can we find the software related to this note?

Thanks.

Regards,

Kamil
Kamil Alkhouri
Associate II
April 17, 2018
Posted on April 17, 2018 at 12:47

Dear Dennis,

I'm also searching for the same stack that supports IEEE 1588 PTPd. It's mentioned in AN3411 Application note which is surprisingly also not available on ST website. Did you find it already? Can you update me regarding this issue?

Regards,

Kamil
Tesla DeLorean
Guru
August 1, 2018

@Szymon PANECKI​ 

It can be found here http://www.bdtic.com/download/ST/AN3411.pdf

People still looking for the PTP examples described therein

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Steven Keeter
Associate III
October 3, 2018

Has the sample code been located by anyone? I actually am looking to port it to the F7 core. I see references to LwIP possibly including a PTPd stack but haven't found anything.

Tesla DeLorean
Guru
October 3, 2018

@STOne-32​ The support for IEEE-1588 continually gets put in to diagrams and slide decks, but there seems to be a consistent lack of delivery for specific/worked examples of its use/application. Can we get someone within ST to take ownership of this issue?

0690X000006C7e5QAC.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
cwparker
Associate II
February 6, 2019

The hardware for IEEE 1588 exists in SMT32Fxxx, so why can't ST document it and provide software examples? AN3411, and demonstration software mentioned in it, shows IEEE 1588 support, but they are no longer available. Why?

I haven't implemented IEEE 1588, but I have used the PTP hardware to synchronize ​STM32F427 uPs on a standard Ethernet switch. To do IEEE 1588 properly, you need switches that support IEEE 1588 boundary clocks to insert actual switching delays into IEEE 1588 packets going through the switch. ST PTP register documentation lists sniffing support for IEEE 1588 packets, but there is no documentation that I can find on that support. Using a standard switch, I get synchronization to about +/- 50 ns (depending on crystal freq. accuracy, switch used and amount of other Ethernet traffic). You can tune this to get even better accuracy. This would most likely be a little better on the H7 at 400MHz.

Note: If you directly connect (no switch) a master and slave uPs for testing, you can better see how the crystal freq. accuracy affects results for your PTP implementation.

Tesla DeLorean
Guru
February 6, 2019

Timing seems to be considered rather niche, or ST lacks domain expertise.

I think the Ethernet IP comes from Synopsys , so other platforms might use it and have some more evolved examples.

The lack of PTP support has been brought up numerous times here, I think it needs a customer large enough to break some legs to get some eyes on the issue.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
anotherandrew
Senior
May 6, 2019

The AN3411 code seems to be largely lost to the sands of time. This is rather disappointing, as STMicro should not ever lose code to their own application notes!

I have found a github repo at https://github.com/mpthompson/stm32_f4_ptpd which seems to include enough of the AN3411 code that you could get it working without too much work. I am using this repo as the basis for my STM32F7 port. It's so far straightforward but not easy. It's also kind of disappointing in STMicro that their HAL has no support for the timestamping functions in their devices. I would have thought I'd find some kind of stm32_hal_eth_ex source file for this, but am instead implementing it on my own, based on the code in that repo.

Tesla DeLorean
Guru
May 6, 2019

Yes the discussion comes up on a recurrent basis. There was a thread a few months back where the timing and dividers were discussed, perhaps in the F7 or H7 vein. I need to search some more.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
May 6, 2019

https://community.st.com/s/question/0D50X0000ALw0M2SQJ/can-i-use-the-stm32f4-ptp-clock-without-an-rmii-clock

I'm not 100% convinced with all the math in here, but it was the most interesting PTP related stuff of recent memory.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Dennis Chou
Associate
May 6, 2019
Thank you everyone for chipping in. Really appreciate it.
VTrue
Associate
May 15, 2019

Thank you. But i need in complete PTP project which used the HAL library. No for commerce. Only for precicsion time measurement and management

cwparker
Associate II
May 17, 2019

​I realized that I left out some code (see previous post - nested) that you'll need to understand what I posted. Where I had the ellipses, you'll need:

	uint32_t now = VM_CLOCK;
	int32_t dt = now - ptp_last_update;
	ptp_last_update = now;

Where VM_CLOCK is defined to be TIM5->CNT and timer 5 is setup to have a 1 us tick (1,000,000 counts per second). This is used in:

	float err = (float)raw_err * 500000.0f / (float)dt; // counts / sec

and is the elapsed time in the slave since the last PTP update (it is not the 'dt' in the comments about latency). The above statement adjusts the error based on the actual time between samples (which for my application is roughly 50 ms).