Skip to main content
Carl Troili
Associate
July 3, 2018
Solved

'cp' is not recognized as an internal or extrenal command

  • July 3, 2018
  • 3 replies
  • 1795 views
Posted on July 03, 2018 at 12:41

I try to build and run the 'Test_PIL_IIR_Filter' using Matlab 2018b.

I get the following error:

### Connectivity configuration for referenced model 'IIR_Filter_int32': STM32 PIL ###

### Preparing to start PIL simulation ...

Building with 'lcc-win64'.

'cp' is not recognized as an internal or external command,

operable program or batch file.

What could be the cause of this.

#SIMULINK

What should I do in order to run the simulation

Regards

This topic has been closed for replies.
Best answer by AvaTar
Posted on July 03, 2018 at 13:21

CP would suggest the expectation of a UNIX/CYGWIN type environment being installed.

Assuming an Unix emulation environment, you probably need to install additional packages. 'cp' was, if I remember correctly, part of binutils.

3 replies

Tesla DeLorean
Guru
July 3, 2018
Posted on July 03, 2018 at 12:48

lcc-win64, sure you've picked the right target compiler here?

CP would suggest the expectation of a UNIX/CYGWIN type environment being installed.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AvaTar
AvaTarBest answer
Senior III
July 3, 2018
Posted on July 03, 2018 at 13:21

CP would suggest the expectation of a UNIX/CYGWIN type environment being installed.

Assuming an Unix emulation environment, you probably need to install additional packages. 'cp' was, if I remember correctly, part of binutils.

Carl Troili
Associate
July 3, 2018
Posted on July 03, 2018 at 13:44

Tried to install CYGWIN and after restarting my computer it did work.

Thanks