Skip to main content
Arman Ilmak
Senior
March 3, 2018
Question

HAL DIVERS for stm8 series?

  • March 3, 2018
  • 6 replies
  • 2536 views
Posted on March 03, 2018 at 17:08

Hey guys.I was just working with stm32f2 series and used cube mx to generate the code,but stm8 series do not have code generator in cube mx(sad

:(

).

I wanted to see if there is any HAL divers or i have to write the code with cmsis?

    This topic has been closed for replies.

    6 replies

    Arman Ilmak
    Senior
    March 3, 2018
    Posted on March 03, 2018 at 17:14

    One more question. Doesn't keil support stm8 series?

    Philipp Krause
    Senior II
    March 3, 2018
    Posted on March 03, 2018 at 20:04

    Keil does not support STM8. Basically, the C compiler choices are: SDCC, IAR, Cosmic, Raisonance. There is a

    http://colecovision.eu/stm8/compilers.shtml

    , but it only considers aspects of the C compilers themselves (i.e. it doesn't consider IDE integration, etc).

    Philipp

    Tesla DeLorean
    Guru
    March 3, 2018
    Posted on March 03, 2018 at 18:01

    The STM8 is not an ARM based core and does not support CMSIS, or Keil.

    The HAL is rather a thick abstraction, and not terribly well suited to something where you want the code as small and fast as possible.

    You want HAL/CubeMX, consider a Cortex-M0(+) based device from the STM32 family.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Arman Ilmak
    Senior
    March 3, 2018
    Posted on March 03, 2018 at 20:19

    You mean it's better to write the code with registers mentioned in the user manual?

    henry.dick
    Associate II
    March 3, 2018
    Posted on March 03, 2018 at 21:57

    The answer depends on your definition of 'better'.

    Working on the registers forces you to understand the device. It is generally more efficient. 

    Whether that's good is up to you.