Why I get STM32H7 GPIO Toggle speed just only at 16.7MHz?
I used NUCLEO-H743ZI board which is mounted STM32H743ZIT, and used STM32 CubeMX generate Code like this.
I config PC9 = MCO2 to output SYSCLK/10. I can get 80MHz wave at Pin PC9, so I ensure the SYSCLK is 400MHz 。 As the AHBCLKDivider = RCC_HCLK_DIV2,so AHB4CLK is 200MHz,。 But I just only get 16.7MHz wave at the Pin PB8. What is wrong with that? Thanks!
void main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
HAL_EnableCompensationCell();while (1){ GPIOB->ODR = 0X100; GPIOB->ODR = 0X00; GPIOB->ODR = 0X100; GPIOB->ODR = 0X00; GPIOB->ODR = 0X100; GPIOB->ODR = 0X00; GPIOB->ODR = 0X100; GPIOB->ODR = 0X00; }}
void SystemClock_Config(void)
{RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;/**Supply configuration update enable
*/MODIFY_REG(PWR->CR3, PWR_CR3_SCUEN, 0);/**Configure the main internal regulator output voltage
*/__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);while ((PWR->D3CR & (PWR_D3CR_VOSRDY)) != PWR_D3CR_VOSRDY)
{}
/**Initializes the CPU, AHB and APB busses clocks*/RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;RCC_OscInitStruct.HSEState = RCC_HSE_ON;RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;RCC_OscInitStruct.PLL.PLLM = 1;RCC_OscInitStruct.PLL.PLLN = 100;RCC_OscInitStruct.PLL.PLLP = 2;RCC_OscInitStruct.PLL.PLLQ = 2;RCC_OscInitStruct.PLL.PLLR = 2;RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;RCC_OscInitStruct.PLL.PLLFRACN = 0;if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK){_Error_Handler(__FILE__, __LINE__);}/**Initializes the CPU, AHB and APB busses clocks
*/RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{_Error_Handler(__FILE__, __LINE__);}HAL_RCC_MCOConfig(RCC_MCO2, RCC_MCO2SOURCE_SYSCLK, RCC_MCODIV_5);
/**Configure the Systick interrupt time
*/HAL_SYSTICK_Config(SystemCoreClock/1000);/**Configure the Systick
*/HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}static void MX_GPIO_Init(void)
{GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOH_CLK_ENABLE();__HAL_RCC_GPIOC_CLK_ENABLE();/*Configure GPIO pin : PC9 */
GPIO_InitStruct.Pin = GPIO_PIN_9;GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;GPIO_InitStruct.Pull = GPIO_NOPULL;GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;GPIO_InitStruct.Alternate = GPIO_AF0_MCO;HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin : PB8 */
GPIO_InitStruct.Pin = GPIO_PIN_8;GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;GPIO_InitStruct.Pull = GPIO_PULLUP;GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);}