Skip to main content
sam Zeng
Associate
Mar 2, 2018 7:13 AM UTC
Question

how to use STM32F407 controll DSP

Posted on March 02, 2018 at 08:13

Now we want to use STM32F407 to control DSP, DSP with 16bit data ports and 5 address,  the following is interface   for DSP, is it okay or not?

#stm32f407
This topic has been closed for replies.

4 replies

AvaTar
Senior III
Mar 2, 2018 7:59 AM UTC
Posted on March 02, 2018 at 08:59

Not sure what you mean.

The CMSIS DSP library is a collection of digital signal processing routines, and of course there is one available for the F40x MCUs.

Be aware that DSP algorithms and some DSP instructions do not make a 'real' DSP.

sam Zeng
sam ZengAuthor
Associate
Mar 3, 2018 2:56 AM UTC
Posted on March 03, 2018 at 03:56

Thank you Avatar, our project is STM32F407XX+DSP, will use  the controller of 

FSMC mode . Is it okay? Thank you very much.

waclawek.jan
Super User
Mar 3, 2018 9:10 AM UTC
Posted on March 03, 2018 at 09:10

FSMC is designed to control external memories. If the DSP chip behaves as an external memory (e.g. it has 16 data bits, several address bits, /RD, /WR and /CS inputs), then it is most probably OK. There still may be details which would prevent this from working, for example some timing constraints, so it's impossible to tell for sure without looking into the datasheet of the DSP chip.

JW

Andrew Neil
Super User
Mar 3, 2018 10:09 AM UTC
Posted on March 03, 2018 at 11:09

You really haven't given enough information about your project for anyone to be able to help much.

Here is the standard approach to interfacing anything to anything else:

http://www.8052.com/forum/read/160143

  
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.