2018-06-28 10:09 AM
On STM32F7, the HS interface has 16 host channels.
But in the HAL, the HCD_HCTypeDef structure has only 15 HCD_HCTypeDef items.
Is this normal ?
Is this a bug ?
Is there an hidden reason ?
(I have an application which can have the need on the 16 channels because several devices will be connected via a hub)
#hcd_handletypedef #hcd_hctypedef2018-07-05 6:23 AM
Hi
ANDRE.THEVENIN
?,The issue is confirmed. We will fix it and update the &39&39stm32f7xx_hal_hcd.h&39&39 ASAP.
Many thanks for bringing this point to our attention
I also advise you to refer to the application note
https://www.st.com/resource/en/datasheet/stm32f479ii.pdf
which will help you to build your own USB application based on an STM32 MCU. If you have any feedback about the application note, please do not hesitate to share it here:https://community.st.com/0D50X00009XkVtDSAV
On the FAQs section, the following question was answered:
Khouloud.