Skip to main content
hesam moshiri
Associate III
July 4, 2018
Question

The ADC of the STM32F103C8 in Dual Simultaneous mode

  • July 4, 2018
  • 0 replies
  • 451 views
Posted on July 04, 2018 at 11:39

Hi,

I have an STM32F103C8 MCU which has two ADC unit peripherals. Each ADC unit can reach up to 1Msps speed or 1uS time resolution.

Can I increase this to 2Msps or 0.5uS by activating the Dual simultaneous mode? if Yes, which option must be selected? (I attached an image from the drop-down list which the mode could be selected

of course data fetch for a single DMA could reach up to 1Mspd, but I'm not quite sure to what speed an ADC can reach in the dual mode.

0690X00000603izQAA.jpg
    This topic has been closed for replies.