Skip to main content
Tung Nguyen
Associate II
July 14, 2018
Question

NACK when program the flash using JLink_Lite

  • July 14, 2018
  • 1 reply
  • 556 views
Posted on July 14, 2018 at 20:38

Hi,

Communication: I2C

Master: STM32F746NGH6

Slave: bq25895M

IDE: Eclipse Neon

Previously, I can read from and write to the slave using HAL_I2C_Mem_Read() and HAL_I2C_Mem_Write() with I2C communication. 

After I program my flash using JFlashLite, my previous program did not work anymore. Particularly, the above methods return HALL_ERROR since NACK flag is set. 

The weird thing is that I have tested if I can get I2C communication using putty, and there is a communication. It just isn't with my previous program.

I don't know why and how to fix this.

Any helps would be appreciated.  

I have included the log from putty in case if its needed for the problem-solving process. 

Test finished successfully. 2

I2C OK with battery charger.

DATA0 IS WRITTEN

DATA1 IS WRITTEN

DATA0 = 0X7F

DATA1 = 0X5

DATA2 = 0X31

DATA3 = 0XA

DATA4 = 0X20

DATA5 = 0X13

DATA6 = 0X82

DATA7 = 0X9D

DATA8 = 0X3

DATA9 = 0X44

DATA10 = 0X93

DATA11 = 0XC6

DATA12 = 0

DATA13 = 0X57

DATA14 = 0

DATA15 = 0

DATA16 = 0

DATA17 = 0XE1

DATA18 = 0

DATA19 = 0X3F

Thanks. 

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    July 14, 2018
    Posted on July 14, 2018 at 21:35

    Going to be hard to troubleshoot remotely.

    I'd assume it's unrelated to the JLink unless you can make a case for something in flash or option bytes interfering with things.

    You need to scope the I2C pins and validate the signals and sequencing. The slave device must respond to it's address on the bus, so the lack of ACK signal indicates the slave is unresponsive. Make sure you have suitable pull ups on the SDA/SCL pins, and the address presents correctly. Check any address jumpers on the slave.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..