NACK when program the flash using JLink_Lite
Hi,
Communication: I2C
Master: STM32F746NGH6
Slave: bq25895M
IDE: Eclipse Neon
Previously, I can read from and write to the slave using HAL_I2C_Mem_Read() and HAL_I2C_Mem_Write() with I2C communication.
After I program my flash using JFlashLite, my previous program did not work anymore. Particularly, the above methods return HALL_ERROR since NACK flag is set.
The weird thing is that I have tested if I can get I2C communication using putty, and there is a communication. It just isn't with my previous program.
I don't know why and how to fix this.
Any helps would be appreciated.
I have included the log from putty in case if its needed for the problem-solving process.
Test finished successfully. 2
I2C OK with battery charger.
DATA0 IS WRITTEN
DATA1 IS WRITTEN
DATA0 = 0X7F
DATA1 = 0X5
DATA2 = 0X31
DATA3 = 0XA
DATA4 = 0X20
DATA5 = 0X13
DATA6 = 0X82
DATA7 = 0X9D
DATA8 = 0X3
DATA9 = 0X44
DATA10 = 0X93
DATA11 = 0XC6
DATA12 = 0
DATA13 = 0X57
DATA14 = 0
DATA15 = 0
DATA16 = 0
DATA17 = 0XE1
DATA18 = 0
DATA19 = 0X3F
Thanks.